10:00 am – 10:40 am
Presenter: Mike Felato, STMicroelectronics
In this session we will discuss various electric vehicle (EV) charging requirements and solutions as well as the topologies and the power semiconductor device types required to create them.
10:50 am – 11:30 am
Presenter: Mike Felato, STMicroelectronics
In this session we will discuss the reasons that silicon carbide (SiC) is desirable for use as a wide bandgap semiconductor for MOSFETs and rectifiers, what advantages it offers, its features and benefits and what power levels and applications see the greatest benefit versus other semiconductors. We will also briefly discuss the various package types used and how they take maximum advantage of this technology.
11:40 am – 12:20 pm
Presenter: George Hempt, STMicroelectronics
In this session, we will show you the increase in power density and system efficiency of our GaN-based offline power supply solutions from 50 W up to 400 W. Starting with our ViperGaN solutions, we have compact USB-PD power supplies for 50 W-100 W as well as integration with our eDesignSuite to shorten design cycles. Our MasterGaN family also integrates the driver with our GaN FETs to simplify power supply design from 45 W to 400 W. This session will focus on compact power supplies for USB-PD, industrial, and high voltage LED applications.
2:00 pm – 2:40 pm
Presenter: George Vince, STMicroelectronics
Teseo dual- and triple-band precise positioning portfolio is designed to cater to ADAS and autonomous navigation applications that demand centimeter or decimeter level accuracy. Based on application requirements various system level architectures will be discussed, emphasizing the scalability and flexibility that differentiates Teseo solutions from competition.
Teseo single-band solutions include LIV3x and VIC3x modules that abstract the complexity of GNSS implementation enabling easy design for faster time-to-market. Teseo single-band standard position solution is suited for asset and fleet tracking applications such as insurance, goods tracking, tolling, anti-theft systems, people and pet location, vehicle tracking, emergency calls, fleet management, vehicle sharing, diagnostics, and public transportation.
By showcasing Teseo's comprehensive range of offerings, this presentation aims to demonstrate cutting-edge solutions for both precise and standard positioning needs.
2:50 pm – 3:30 pm
Presenter: George Hempt and/or Allan Soriano, STMicroelectronics
ST is releasing system solutions for wireless charging and wireless power transfer applications, from 2.5W to over 100W. Wireless charging is not a new technology; however, our solutions solve unique application and design problems. Our solutions are integrated, provide monolithic Rx and Tx ICs to minimize BOM cost and shrink devices that use our ICs.
In this session, we will cover the wireless power IC portfolio, system designs, and a user-friendly GUI to kickstart your design process, reduce BOM cost, while maintaining strong system efficiency in a truly wireless system.
3:40 pm – 4:20 pm
Presenter: Mounik Rupani, STMicroelectronics
Precision operational amplifiers are the primary link between many accurate analog sensors used to measure temperature, speed, pressure, UV, etc. and the digital world. This session will highlight the parameters of an op-amp that are key for its precision, with examples and how ST op-amps can solve problems in this regard.
4:30 pm – 5:30 pm
Presenter: Mounik Rupani, STMicroelectronics
This power tree design session will show how ST devices can be used to build a full power solution with multiple low voltage DC power rails. Highlights will include a deep dive of step-down DC/DC switching converter operation, an overview of ST step-down DC/DC switching converters, and live demos of the eDesignSuite Power Tree Tool and eDSim simulation tool.
10:00 am – 10:40 am
Presenter: Prasad Golla, STMicroelectronics
ST4SIM is an ST-initiated program to provide connectivity to M2M/IoT devices through connectivity partners including MNOs like Verizon, AT&T and other carriers in the North American region, and also MVNOs able to provide connectivity across the globe. AT ST, we produce the silicon loaded with the smartcard operating system in certified secure personalization centers. eSIM IOT is compliant with SGP.32 specifications and is available in various form factors and multiple silicon grades. eSIM IOT is capable of swapping carriers of choice without dependencies for use-cases like late-stage personalization or in a production line at the device manufacturing facility.
10:50 am – 11:30 am
Presenter: Colin Ramrattan, STMicroelectronics
Connecting smart home devices has always been a challenge with different devices from different manufacturers. Matter is the simplification of the connectivity standards making it easy for consumers to connect all of their devices and enable seamless compatibility. STMicroelectronics is fully committed to supporting Matter, and STM32WB5x devices enable this connectivity.
11:40 am – 12:20 pm
Presenter: John Kvam, STMicroelectronics
Join us to discover how ST can help you make use of invisible light to enhance your application, enrich your device capabilities or increase your automation processes efficiency.
You will be introduced to our latest Time-of-Flight (ToF) sensors, the VL53L7CX and VL53L8CX; have an overview of the newest applications and use-cases that we have focused on recently, as well as an update on the availability and the powerful ecosystem ST is offering to his customers.
2:00 pm – 2:40 pm
Presenter: Tom Bocchino/TBD, STMicroelectronics
In this session, we'll discuss two complementary presence detection sensor technologies from ST aiming at making your devices more intelligent and power efficient.
The TMOS STHS34PF80 is an uncooled, low-power, factory-calibrated IR sensor with operating wavelength between 5 µm and 20 µm designed to sense presence based on the absolute temperature of objects within its field-of-view (FoV).
From low-power single-zone to multi-zone depth sensors, the FlightSense™ family enables accurate depth measurements and advanced features such as passing-by, touchless control, and people counting.
ST sensor solutions for presence detection make devices more intelligent and power efficient.
2:50 pm – 3:30 pm
Presenter: Manuel Cantone, STMicroelectronics
In this session, we will introduce the technologies ST is leveraging to keep the lead in Motion MEMS Technologies.
The LSM6DSV Inertial Measurement Unit (IMU) family merges high-performance and ultra-low-power while bringing new advanced features like High Accuracy ODR, Sensor Fusion Low-power, Advanced Processing in the Edge with second generation Finite State Machine (FSM), Machine Learning Core (MLC) and Adaptive System Configuration (ASC). In addition, an embedded Qvar (electric charge variation detection) channel can be enabled for sensing in applications such as touch, long press, and L/R - R/L swipe.
MLC, FSM, ASC and Qvar can also be found in the latest Accelerometer LIS2DUXS12.
The Intelligent Sensor Processing Unit (ISPU) equipped IMUs offer instead an ultra-low power, high-performance, and user-programmable DSP core designed to utilize the tinyML ecosystem tools and open-source development resources to fully customize the behavior of the sensor. Some examples are provided in the X-CUBE-ISPU package and anomaly detection algorithms can be programmed with NanoEdge.AI.
3:40 pm – 4:20 pm
Presenter: Alexandra Gogonea, STMicroelectronics
ST’s pressure sensors are increasingly being used in smartphones, tablets, and wearable technology such as sports watches, smart watches, and fitness bands, enabling accurate floor detection and enhanced location-based services, allowing more accurate dead-reckoning calculations, and opening the door to new industrial applications, like smart flow detectors and predictive maintenance.
This new generation of sensors embed an analog hub sensing functionality which is capable of connecting an analog input and converting it to a digital signal for embedded processing. In addition, an embedded Qvar (electric charge variation detection) channel can be enabled for sensing in applications such as water leakage detection, tap, double-tap, long press, and L/R - R/L swipe.
4:30 pm – 5:30 pm
Presenter: Manuel Cantone/Michael Hess, STMicroelectronics
The STEVAL-MKBOXPRO (SensorTile.box PRO) is the new ready-to-use wireless box kit for developing any IoT application based on remote data gathering leveraging motion, environmental data sensing and sound with a digital microphone.
The Kit is designed to be used according to three different modalities:
10:00 am – 10:40 am
Presenter: Stefanie Lau or Tim Nakonsut, STMicroelectronics
ST has recently released the new STM32H5 and an updated lineup on the STM32U5 microcontrollers. Both families offer advanced features such as graphics, hardware accelerators, and digital signal processing, as well as a range of communication interfaces, memory options, and security features.
10:50 am – 11:30 am
Presenter: Stefanie Lau or Tim Nakonsut, STMicroelectronics
The STM32MP13x is ST’s latest MPU solution that utilizes our OpenSTLinux distribution to help designers looking to develop embedded systems with enhanced security at a low cost.
11:40 am – 12:20 pm
Presenter: Tim Nakonsut, STMicroelectronics
In this session, we will demonstrate the STM32 IoT cloud solutions which are secure, reliable, and scalable to start your next IoT project. We will then focus on the IoTConnect platform from Avnet, which securely connects the low-power STM32U5 to the cloud.
The session will include a brief overview of the latest STM32 IoT Edge roadmap, followed by a demo of the STM32U5 running Microsoft Azure RTOS and Trusted Firmware-M. The device will securely connect to Azure using Avnet’s IoTConnect platform and the STSAFE secure element. Additionally, we will walk through a step-by-step Quick Start to create a Proof-of-Concept (PoC) leveraging the many ST sensors available on the B-U585I-IOT02A STM32U5 Discovery Kit for IoT Node.
From this session, we hope you will be able to understand, discover, and get everything you need to power your IoT product – from device to cloud to actionable insights.
2:00 pm – 2:40 pm
Presenter: Colin Ramrattan, STMicroelectronics
Bluetooth LE connectivity is becoming more common as the world becomes more connected. To meet the needs of IoT device manufacturers and their customers, ultra-low power consumption and advanced security are essential, with SESIP certification often being a requirement. Discover the STM32WBA52 Wireless SoC that excels at these requirements for your wireless design
2:50 pm – 3:30 pm
Presenter: Louis Gobin, STMicroelectronics
ST's STM32Cube.AI Developer Cloud is the latest platform from ST for machine learning development for microcontrollers. Combined with ST's model zoo this platform will let you optimize, compile, and test your model's remotely on ST's board farm for real world performance metrics on a wide variety of different STM32 platforms so you can test, iterate, and optimize for both cost and performance without having to buy your target board.
3:40 pm – 4:20 pm
Presenter: Stefanie Lau or Tim Nakonsut, STMicroelectronics
ST has recently released the new STM32H5 and an updated lineup on the STM32U5 microcontrollers. Both families offer advanced features such as graphics, hardware accelerators, and digital signal processing, as well as a range of communication interfaces, memory options, and security features.
4:30 pm – 5:30 pm
Presenter: Jim Barlow/John Tran, STMicroelectronics
NFC solutions based on STEVAL-SMARTAG2, a NFC-enabled sensor and processing node featuring Dynamic NFC Tag, environmental, motion, and ambient light sensors with cryptographic security, enables ultra-low power IoT applications by transmitting sensor data via NFC using energy harvesting and wireless charging capability.
10:00 am – 1:00 pm
Presenter: Louis Gobin and Allen Ren, STMicroelectronics
NanoEdge AI Studio is a development environment that makes it easy to create machine learning (ML) algorithms for any STM32 microcontroller.
In this hands-on workshop, you will learn how to create a predictive maintenance application on a smart IoT device using current, thanks to NanoEdge AI Studio.
In the lab sessions, you will use NanoEdge AI Studio to develop a machine learning algorithm, and the STM32CubeIDE Integrated Development Environment to implement your library quickly and easily on an STM32 microcontroller. The ST technical team will be there to guide you through each step in the process.
Prerequisites for participation in this workshop:
The development boards required for the lab sessions will be provided by STMicroelectronics for use during the workshop and collected at the end of the training.
Due to seating limitations, this workshop requires separate registration. Note that registering for this workshop also grants you full access to the ST Technology Tour event, including the technology demos, presentations, lunch, and refreshments.
2:00 pm – 5:30 pm
Presenter: Stefanie Lau and Emily Bowdach, STMicroelectronics
Could your next 8-bit MCU be a 32-bit?
Join us for a hands-on workshop to learn how to upgrade your next cost-sensitive application with STM32C0 using our STM32 Nucleo-64 development board.
We will guide you through hands-on demos and show you how to use ST’s extensive development ecosystem to fast-track your designs.
This workshop is intended for 8-bit, 16-bit and 32-bit engineers, firmware developers, and hardware design engineers of all levels looking to design with an affordable, future-ready MCU from the STM32 family of microcontrollers.
Prerequisites for participation in this workshop:
An STM32 Nucleo-64 development board will be provided by STMicroelectronics for use during the lab sessions and collected at the end of the training.
Due to seating limitations, this workshop requires separate registration. Note that registering for this workshop also grants you full access to the ST Technology Tour event, including the technology demos, presentations, lunch, and refreshments.
Premier
Featured
Lorem ipsum dolor sit amet, consectetur adipisicing elit.
Premier
Featured