10:00 am – 10:40 am
Presenter: George Vince, STMicroelectronics
Teseo dual- and triple-band precise positioning portfolio is designed to cater to ADAS and autonomous navigation applications that demand centimeter or decimeter level accuracy. Based on application requirements various system level architectures will be discussed, emphasizing the scalability and flexibility that differentiates Teseo solutions from competition.
Teseo single-band solutions include LIV3x and VIC3x modules that abstract the complexity of GNSS implementation enabling easy design for faster time-to-market. Teseo single-band standard position solution is suited for asset and fleet tracking applications such as insurance, goods tracking, tolling, anti-theft systems, people and pet location, vehicle tracking, emergency calls, fleet management, vehicle sharing, diagnostics, and public transportation.
By showcasing Teseo's comprehensive range of offerings, this presentation aims to demonstrate cutting-edge solutions for both precise and standard positioning needs.
10:50 am – 11:30 am
Presenter: Nicolò Boni, STMicroelectronics
Advanced Inertial MEMS Sensors with embedded capabilities such as Machine Learning Core (MLC), Finite State Machine (FSM), and ASIL-B Certification are key pillars for traditional and emerging applications in the transportation market segment. Leveraging MLC capabilities can enable unique solutions such as theft detection without the intervention of main processor or microcontroller.
11:40 am – 12:20 pm
Presenters: John Johnson & Khaldoun Albarazi, STMicroelectronics
This session covers ST's broadly- deployed, full-production automotive MCU portfolio based on the Power PC core architecture. We will also cover electrification- and zone-focused ARM-based MCU roadmap that addresses the needs of future automobile architectures.
2:00 pm – 2:40 pm
Presenter: Cosimo Leonardi, STMicroelectronics
In this session we will discuss the reasons that silicon carbide (SiC) is desirable for use as a wide bandgap semiconductor for MOSFETs and rectifiers, what advantages it offers, its features and benefits and what power levels and applications see the greatest benefit versus other semiconductors. We will also briefly discuss the various package types used and how they take maximum advantage of this technology.
2:50 pm – 3:30 pm
Presenter: Yaya Liu, STMicroelectronics
In this session, we will show you the increase in power density and system efficiency of our GaN-based offline power supply solutions from 50 W up to 400 W. Starting with our ViperGaN solutions, we have compact USB-PD power supplies for 50 W-100 W as well as integration with our eDesignSuite to shorten design cycles. Our MasterGaN family also integrates the driver with our GaN FETs to simplify power supply design from 45 W to 400 W. This session will focus on compact power supplies for USB-PD, industrial, and high voltage LED applications.
3:40 pm – 4:20 pm
Presenter: George Hempt, STMicroelectronics
Gate drivers are a critical piece of any high voltage converter system. ST has been developing key technologies to drive everything from IGBTs and Silicon MOSFETs, to wide bandgap GaN and SiC FETs. From our STDRIVE family to our galvanic isolated STGAP family, ST has gate driving solutions and reference designs from hundreds of watts to tens of kilowatts. This session will cover our gate driver family and how to create reliable and efficient switching converters.
10:00 am – 10:40 am
Presenter: Matteo Fusi, STMicroelectronics
In this session, we will introduce the technologies ST is leveraging to keep the lead in Motion MEMS Technologies.
The LSM6DSV Inertial Measurement Unit (IMU) family merges high-performance and ultra-low-power while bringing new advanced features like High Accuracy ODR, Sensor Fusion Low-power, Advanced Processing in the Edge with second generation Finite State Machine (FSM), Machine Learning Core (MLC) and Adaptive System Configuration (ASC). In addition, an embedded Qvar (electric charge variation detection) channel can be enabled for sensing in applications such as touch, long press, and L/R - R/L swipe.
MLC, FSM, ASC and Qvar can also be found in the latest Accelerometer LIS2DUXS12.
The Intelligent Sensor Processing Unit (ISPU) equipped IMUs offer instead an ultra-low power, high-performance, and user-programmable DSP core designed to utilize the tinyML ecosystem tools and open-source development resources to fully customize the behavior of the sensor. Some examples are provided in the X-CUBE-ISPU package and anomaly detection algorithms can be programmed with NanoEdge.AI, and Machine Learning based classification can be implemented with the help of ST’s partner Neuton.AI Auto ML
10:50 am – 11:30 am
Presenter: George Hempt, STMicroelectronics
ST is a global leader in solutions for connected grid systems, both for local residential energy system micro grids and larger-scale infrastruture systems. This session will provide an introduction to wired power line communication systems, hybrid wired + sub-GHz wireless systems, as well as metering solutions.
11:40 am – 12:40 pm
Presenter: Victor Ceron, STMicroelectronics
This power tree design session will show how ST devices can be used to build a full power solution with multiple low voltage DC power rails. Highlights will include a deep dive of step-down DC/DC switching converter operation, an overview of ST step-down DC/DC switching converters, and live demos of the eDesignSuite Power Tree Tool and eDSim simulation tool.
2:50 pm – 3:30 pm
Presenter: John Johnson, STMicroelectronics
For battery operated products, lithium-ion battery chemistry is a mixed blessing. Consumers want products that charge quickly, operate for long periods of time, are safe and reliable, and perhaps most importantly are cost effective. Lithium-ion batteries have many intrinsic qualities that help engineers achieve these design objectives. However, lithium-ion cells are finicky to manage; and battery management system (BMS) designs require a lot of attention to detail.
In this session, we will explore the qualities of lithium-ion cells and the hardware and algorithms necessary to manage them. We will examine various BMS architectures and the trade-offs associated with each approach. We will explore some basics of how to estimate parameters like state of charge and state of health. We will round out our discussion with an introduction to some of the products offered by STMicroelectronics that help engineers build state-of-the-art BMS.
2:00 pm – 2:40 pm
Presenter: Cosimo Leonardi, STMicroelectronics
In this session we will discuss various electric vehicle (EV) charging requirements and solutions as well as the topologies and the power semiconductor device types required to create them.
3:40 pm – 4:20 pm
Presenter: Sara Mattioli, STMicroelectronics
Take your power distribution and control solution to the next level with ST's latest high side drivers in VIPower™ M09 Technology and STi2Fuse ICs, enabling lower cost, increased reliability, and more intelligent circuit designs. Ideal for a multitude of applications in the automotive, transportation, industrial, medical, and consumer electronics spaces.
10:00 am – 10:40 am
Presenter: Jim Barlow, STMicroelectronics
In this session, we will present NFC solutions based on the STEVAL-SMARTAG2, an NFC-enabled sensor and processing node featuring a Dynamic NFC Tag, environmental, motion, and ambient light sensors with cryptographic security, which enable ultra low-power IoT applications by transmitting sensor data via NFC using energy harvesting and wireless charging capabilities.
10:50 am – 11:30 am
Presenter: Jim Barlow, STMicroelectronics
ST4SIM is an ST-initiated program to provide connectivity to M2M/IoT devices through connectivity partners including MNOs like Verizon, AT&T and other carriers in the North American region, and also MVNOs able to provide connectivity across the globe. AT ST, we produce the silicon loaded with the smartcard operating system in certified secure personalization centers. eSIM IOT is compliant with SGP.32 specifications and is available in various form factors and multiple silicon grades. eSIM IOT is capable of swapping carriers of choice without dependencies for use-cases like late-stage personalization or in a production line at the device manufacturing facility.
11:40 am – 12:20 pm
Presenter: Ernesto Manuel Cantone, STMicroelectronics
The STEVAL-MKBOXPRO (SensorTile.box PRO) is the new ready-to-use wireless box kit for developing any IoT application based on remote data gathering leveraging motion, environmental data sensing and sound with a digital microphone.
The Kit is designed to be used according to three different modalities:
2:00 pm – 2:40 pm
Presenter: Alexandra Gogonea and Ruchi Upadhyay, STMicroelectronics
In this session, we'll discuss two complementary presence detection sensor technologies from ST aiming at making your devices more intelligent and power efficient.
The TMOS STHS34PF80 is an uncooled, low-power, factory-calibrated IR sensor with operating wavelength between 5 µm and 20 µm designed to sense presence based on the absolute temperature of objects within its field-of-view (FoV).
From low-power single-zone to multi-zone depth sensors, the Time-of-Flight family enables accurate depth measurements and advanced features such as passing-by, touchless control, and people counting.
ST sensor solutions for presence detection make devices more intelligent and power efficient.
2:50 pm – 3:30 pm
Presenter: Colin Ramrattan, STMicroelectronics
Bluetooth LE connectivity is becoming more common as the world becomes more connected. To meet the needs of IoT device manufacturers and their customers, ultra-low power consumption and advanced security are essential, with SESIP certification often being a requirement. Discover the STM32WBA52 Wireless SoC that excels at these requirements for your wireless design
3:40 pm – 4:20 pm
Presenter: Yaya Liu, STMicroelectronics
ST is releasing system solutions for wireless charging and wireless power transfer applications, from 2.5W to over 100W. Wireless charging is not a new technology; however, our solutions solve unique application and design problems. Our solutions are integrated, provide monolithic Rx and Tx ICs to minimize BOM cost and shrink devices that use our ICs.
In this session, we will cover the wireless power IC portfolio, system designs, and a user-friendly GUI to kickstart your design process, reduce BOM cost, while maintaining strong system efficiency in a truly wireless system.
10:00 am – 10:40 am
Presenter: Louis Gobin or Miguel Castro, STMicroelectronics
ST's STM32Cube.AI Developer Cloud is the latest platform from ST for machine learning development for microcontrollers. Combined with ST's model zoo this platform will let you optimize, compile, and test your model's remotely on ST's board farm for real world performance metrics on a wide variety of different STM32 platforms so you can test, iterate, and optimize for both cost and performance without having to buy your target board.
10:50 am – 11:30 am
Presenter: Colin Ramrattan, STMicroelectronics
Connecting smart home devices has always been a challenge with different devices from different manufacturers. Matter is the simplification of the connectivity standards making it easy for consumers to connect all of their devices and enable seamless compatibility. STMicroelectronics is fully committed to supporting Matter, and STM32WB5x devices enable this connectivity.
11:40 am – 12:20 pm
Presenter: John Kvam, STMicroelectronics
Join us to discover how ST can help you make use of invisible light to enhance your application, enrich your device capabilities or increase your automation processes efficiency.
You will be introduced to our latest Time-of-Flight (ToF) sensors, the VL53L7CX and VL53L8CX; have an overview of the newest applications and use-cases that we have focused on recently, as well as an update on the availability and the powerful ecosystem ST is offering to his customers.
2:00 pm – 2:40 pm
Presenter: Tim Nakonsut, STMicroelectronics
ST has recently released the new STM32H5 and an updated lineup on the STM32U5 microcontrollers. Both families offer advanced features such as graphics, hardware accelerators, and digital signal processing, as well as a range of communication interfaces, memory options, and security features.
2:50 pm – 3:30 pm
Presenter: Tim Nakonsut, STMicroelectronics
The STM32MP13x is ST’s latest MPU solution that utilizes our OpenSTLinux distribution to help designers looking to develop embedded systems with enhanced security at a low cost.
3:40 pm – 4:20 pm
Presenters: Ramkumar Yadavalli, STMicroelectronics and Trevor Cain, Avnet
In this session, we will demonstrate the STM32 IoT cloud solutions which are secure, reliable, and scalable to start your next IoT project. We will then focus on the IoTConnect platform from Avnet, which securely connects the low-power STM32U5 to the cloud.
The session will include a brief overview of the latest STM32 IoT Edge roadmap, followed by a demo of the STM32U5 running Microsoft Azure RTOS and Trusted Firmware-M. The device will securely connect to Azure using Avnet’s IoTConnect platform and the STSAFE secure element. Additionally, we will walk through a step-by-step Quick Start to create a Proof-of-Concept (PoC) leveraging the many ST sensors available on the B-U585I-IOT02A STM32U5 Discovery Kit for IoT Node.
From this session, we hope you will be able to understand, discover, and get everything you need to power your IoT product – from device to cloud to actionable insights.
10:00 am – 12:00 pm
Presenters: Anis Ben Abdallah & Stefanie Lau, STMicroelectronics
During this workshop, our STM32 experts will provide a complete overview of the performance, communication, and security features of the STM32H5, and explain how they can make a real difference in your design. The best combination of performance and security, in an affordable way!
The STM32H5 MCU sets a new standard for mainstream MCUs, thanks to the most powerful implementation of the Arm Cortex-M33 core running as high as 250 MHz – a first in the MCU world. Reaching a 1017 CoreMark score, the STM32H5 comes with up to 2 Mbytes of flash memory and up to 640 Kbytes of RAM. It also features CORDIC and FMAC accelerators, and is the first STM32 to come with an I3C interface.
We will walk you through an embedded application example based on the STM32H5 so you can see some of its features in action, such as GPIO states retention, the I3C interface, and the GPDMA, and try them out yourself.
Prerequisites for participation in this workshop:
The STM32H5 development board (NUCLEO-H563ZI) required for the lab sessions will be provided by STMicroelectronics for use during the workshop, and collected at the end of the training.
Due to seating limitations, this workshop requires separate registration. Note that registering for this workshop also grants you full access to the ST Technology Tour event, including the technology demos, presentations, lunch, and refreshments.
2:00 pm – 4:00 pm
Presenters: Louis Gobin and Allen Ren, STMicroelectronics
Attendees will learn how to see the world with STM32 microcontrollers using STM32Cube.AI. During the hands-on part of this workshop, a pre-trained neural network model will be ingested in Cube.AI for C-code implementation on an STM32H7 MCU.
This workshop will also empower attendees to adapt existing neural network models for their specific application requirements without having to retrain them from scratch. Transfer learning will be used to recognize and classify a new specific set of objects placed in front of a camera sensor. This workshop will be in person with a team from STMicroelectronics to guide you every step of the way.
STM32Cube.ai and Cube.AI Developer Cloud are STMicroelectronics solution platforms that ease the implementation of deep learning models. They allow one to create and train NN models using their favorite environment for execution on target STM32 MCUs and MPUs. The Cube.AI ecosystem ingests quantized or mixed precision models and delivers unmatched performance and accuracy for every model on the STM32 that’s right for you.
Prerequisites for participation in this workshop:
The development kit required for the lab exercises (STM32H747I-DISCO + B-CAMS-OMV camera module) will be provided by STMicroelectronics for use during the lab sessions, and collected at the end of the training.
Due to seating limitations, this workshop requires separate registration. Note that registering for this workshop also grants you full access to the ST Technology Tour event, including the technology demos, presentations, lunch, and refreshments.
Premier
Featured
Lorem ipsum dolor sit amet, consectetur adipisicing elit.
Premier
Featured