The workshop is based on our latest motion MEMS and environmental sensors expansion board, which is part of the STM32ODE ecosystem (X‑NUCLEO‑IKS4A1). You will learn how to interface with various MEMS sensors, visualize and analyze their data, and take advantage of advanced digital features such as the Machine Learning Core and Intelligent Sensor Processing Unit.
The sensor expansion board features ST's newest and most advanced sensors, including:
We'll use MEMS-Studio, a complete desktop software solution for developing embedded AI features, evaluating embedded libraries, analyzing data, and designing no-code algorithms for the entire MEMS sensor portfolio. This unique software solution offers a versatile development environment for evaluating and programming all MEMS sensors.
This workshop is self-paced and can be accessed on-demand any time after the start of the selected session. However, please note that the live technical support (via online break-out rooms) is available only during the scheduled session hours (see table below).
This workshop is for engineers who want to quickly prototype sensor-based applications and rapidly deploy a proof-of-concept (PoC) for data acquisition.
This workshop is open to residents of the Americas only.
The STM32 Nucleo-64 development board with STM32F401RE MCU (NUCLEO-F401RE) and Motion MEMS and environmental sensor expansion board for STM32 Nucleo (X-NUCLEO-IKS4A1) are required to perform the lab exercises (see Prerequisites).
Exclusively for registrants of this workshop, the boards can be purchased in the ST eStore on a buy one, get the other free basis, with free shipping. You will receive a coupon code and purchase instructions by email shortly after we receive your request to participate.
We recommend using two screens so that you can watch, pause, and rewind the instruction video on one screen while completing the workshop tasks on the other.
Lorem ipsum dolor sit amet, consectetur adipisicing elit.
Sessions (US Eastern Time)
Each session is the complete workshop. Please select only one session when submitting your request to participate.
Date
Time

Michael Hess is Applications Manager for the ST Americas Sensors to Cloud Team. At ST, his career has included managing OEM/ODM and partner relationships for ST’s broad portfolio of MEMS sensors and microcontrollers. Michael earned his B.S. in Electrical Engineering from Manhattan College in NY.
MEMS-Studio facilitates the process of implementing proof-of-concept using a graphical interface without writing code for STM32 microcontrollers. This solution allows configuring sensors and embedded AI (machine learning and neural networks), leveraging on a machine learning core (MLC), neural networks for the ISPU, and finite state machines (FSM). It reuses embedded software libraries, combines multiple functionalities in a single project, and visualizes data in real time using plot and display.
MEMS-Studio is part of the ST Edge AI Suite, which is an integrated collection of software tools, designed to facilitate the development and deployment of embedded AI applications. This comprehensive suite supports both optimization and deployment of machine learning algorithms and neural network models, starting from data collection to final deployment on hardware, streamlining the workflow for professionals across various disciplines.